AXIS#.GEAR.IN
Description
This parameter sets the denominator of the gear ratio for the electronic gearing mode. The gear ratio is used in order to increase and decrease the slave velocity. The slave velocity can be calculated by the following formula:
Slave velocity = Master velocity * AXIS#.GEAR.OUT/AXIS#.GEAR.IN
Be sure that you set the external master source number of signals per revolution correctly. See AXIS#.GEAR.FBSOURCE to determine the gearing master source and verify the feedback resolution for that device.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 65,535 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.GEAR.IN | 0x5006 | 0x3 | UINT | - | - | RW | False |
| AXIS2.GEAR.IN | 0x5106 | 0x3 | UINT | - | - | RW | False |